1/17/2022 4:59 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1047)
|
HI EduOjalvo, try to update the FW of the CPU and the Display. FW-Update can be downloaded here: Firmware update S7-1500 CPUs incl. Displays and ET 200 CPUs (ET 200SP, ET 200pro)hope this helps, regards, |
FCK WAR! |
|
1/17/2022 5:21 PM | |
Joined: 10/26/2011 Last visit: 2/27/2024 Posts: 13 Rating: (0) |
Thank very much. I´ll try it. |
1/18/2022 11:59 AM | |
Joined: 3/11/2019 Last visit: 3/28/2024 Posts: 1308 Rating: (230) |
Hi, you can try to unplug/plug the display again, sometimes this can help. Replacing the display/front cover"The display is pluggable. You can remove or replace the display during operation (RUN). Removing or replacing of the display does not have any influence on the running CPU." Please note the warning if the cpu is used in zone 2. regards sacnruz |
Feedback appreciated, please rate |
|
Follow us on