10/28/2018 5:44 PM | |
Posts: 12 Rating:
|
Hello, We have a large project with 14 S7-1500 PLCs. To manage it easier we started using a project library. The idea was to have ability to instantly update all points of use (called instances). However it appears that types (FBs, FCs, UDT's and simmilar elements in the project library) and their versions is not whole picture. There also is such thing like a type instance and test environment. It is not well explained in the manual, but it looks like a type with same version "x.x.x" can have multiple different type instances. Can someone explain me the how to make all instances of a type identical? In other words: I want to have only one version of UDT_TU in whole project (multiple PLCs). And I want that whenever I update UDT_TU, the changes would be transferred to every PLC in the project and every place where this data type is used. I want to destroy all versions with underscores (like UDT_TU_1). How to achieve that? ------------------------------------------------------------------------------------------ |
Last edited by: tomasDema at: 10/28/2018 5:57:43 PMLast edited by: Jen_Moderator at: 10/29/2018 7:32:28 AMNew subject after splitting |
|
10/29/2018 2:28 PM | |
Joined: 5/28/2008 Last visit: 7/15/2024 Posts: 1343 Rating:
|
Have you seen this: https://support.industry.siemens.com/cs/ww/de/view/109747503/en ? |
This contribution was helpful to
1 thankful Users |
Follow us on