1/24/2022 7:59 AM | |||
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289) |
Dear walter_g, the CPU1511 can handle way more than 32 devices itself, so if you do not need a seperate PROFINET network, you can connect the io-link master modules directyl to the cpu. CPU 1511-1PN, 150KB Program, 1MB Data"
" regards sancruz |
||
Feedback appreciated, please rate |
|||
This contribution was helpful to1 thankful Users |
1/24/2022 6:16 PM | |||||
Joined: 7/5/2006 Last visit: 9/4/2024 Posts: 180 Rating: (4) |
Hello Sancruz, thanks for the reply, but I had seen that the number of IO System is only 32. So the item 6ES7148-6JD00-0AB0 SIMATIC DP, ET 200eco PN, IO-Link master, 4IO-L is an IO Device and not an IO system ? I'm confused, sorry. Can you clarify me please? This is take from CPU1511-1PN datasheet
|
||||
Follow us on