2/9/2022 6:56 PM | |
Joined: 2/19/2013 Last visit: 8/7/2024 Posts: 184 Rating: (8) |
Here you have the content of the UDT: |
2/10/2022 9:04 AM | |
Joined: 9/23/2005 Last visit: 8/7/2024 Posts: 4660 Rating: (718) |
One option is to change your UDT to something like following:
and pass this. If you need multiple queues, you can build an array of this UDT and use indexing to choose one. Other option is to create an FB for handling queue and pass ARRAY[*] OF SomeDataType to it. Then you can have different queues with arbitrary lengths. And finally there's the LGF to save from breaking an open door. |
Regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on