3/27/2009 2:24 PM | |
Joined: 10/18/2006 Last visit: 7/29/2024 Posts: 163 Rating:
|
Hi experts! after starting the OS in the Server, the OS Clients connected to this Server don´t allow faceplates handling. For example, a Simocode faceplate has its buttons disabled, the alarm SP of a Meas_Mon faceplate cannot be changed, etc, etc.
Something similar happens withe alarm messages. The OS Clients don´t recognize the alarms until the alarm screen is opened in the Server and the alarms are acknowledged. If we don´t perform this action, alarms are only acknowledged in the Clients by opening the device faceplate, maximizing all the sub-faceplates and acknowledging them from the alarm sub-faceplate.
AttachmentScreenshots_Freeze.zip (79 Downloads) |
Follow us on