3/26/2022 2:34 PM | |
Joined: 11/28/2018 Last visit: 4/25/2024 Posts: 19 Rating: (0) |
Hi folks I need to generate an excel file through wincc advanced tia portal, with a template excel file and data to stored in desired cell in REAL , INT & STRING format, and finally the excel needs to be converted to .pdf format. I have attached the example template excel below with cells that are variable highlighted in yellow, can anyone share me script or application example for the above requirement , Need it ASAP, help would be highly appreciated AttachmentTEST.xlsx (149 Downloads) |
DeepaK.K |
|
3/26/2022 3:58 PM | |
Joined: 11/28/2018 Last visit: 4/25/2024 Posts: 19 Rating: (0) |
Thank you Obrigado, I'll refer to it |
DeepaK.K |
|
This contribution was helpful to1 thankful Users |
3/30/2022 3:24 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello Beans799 you can use the MS Automatoin interface with VB Script on a PC based Runtime System where Excel is installed. There is only a short example in the WInCC V7 Help System but it works of course also in WinCC Advanced RT and WinCC Prof (NOT on Comfort Panel): https://support.industry.siemens.com/cs/de/en/view/109792622/139193407371 (Of course you have to change the syntax a little bit if you use TIA Portal) Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on