4/11/2022 2:51 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello; Have you set up the Ressources configuration dialog to include a F-CPU in your SIMIT parameters? From the SIMIT Virtual Controller (VC) reference manual: https://support.industry.siemens.com/cs/ww/en/view/107196861/73312764939
Hope this helps, Daniel Chartier |
4/11/2022 3:59 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666) |
Hello; The SIMIT v10.3 manual mentions "F Systems" unit couplings in a few sections, such as you can see in the screenshot below, and in the following quotes for example: • The virtual controller supports the "S7 F Systems Lib V1_3" library and "Safety Matrix" in failsafe operation. Error states cannot be mapped. Only limited use of snapshots is possible in connection with the "S7 F Systems Lib". • "Distributed Safety" is not supported. https://support.industry.siemens.com/cs/ww/en/view/109801804 Hope this helps, Daniel Chartier |
Follow us on