4/26/2022 2:19 PM | |
Joined: 3/9/2021 Last visit: 11/23/2023 Posts: 4 Rating: (0) |
Hi guys, im having troubles with TIA PORTAL V17. I have a KTP700 Basic 6AV2 123-2GB03-0AX0 with TIA 16 on it, but when I upgrade the program to TIA 17 and try to download the program on the TP, this error "Download has failed due to missing panel image" appears and I cant upgrade the TP. I install on my computer the SIMATIC_WinCC_Panel_Images_V17 and I see I have on C:\Program Files\Siemens\Automation\Portal V17\Data\Hmi\Transfer\17.0\Images I have a folder with this KTP700.fwf so I don't know how I can solve this problem... Did you know something more I can do? Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2022 09:30:00New subject after splitting |
|
4/28/2022 12:40 PM | |
Joined: 8/3/2009 Last visit: 10/15/2024 Posts: 13942 Rating: (1757)
|
Hello Carmendomar95 If you install TIa V17 then the Panel Images are not included in main DVD. you have to install the DVD3 with the V17 Panel images If you have already then you will have only the V17 PAnel Files but not older files. Here there is a DVD 4 with Panel legacy images!! LINK Here are the Images <V17 included. After that also the Transfer with a smaller IMage Version should work. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on