2/5/2014 11:07 AM | |
Posts: 3093 Rating: (322)
|
Hello Arian, in most applications I know, Yokogawa is the client. But I'm pretty sure, that Yokogawa can act as client and server as well. It is the first and the main thing to ask when planing a communication which device is client and which server. So ask the programmer of the Yokogawa system. Regards, Kaulquappe |
5/2/2014 6:04 AM | |
Joined: 9/3/2011 Last visit: 4/22/2024 Posts: 24 Rating: (0) |
hello thank you for your reply Finally I found the problem I solved it
|
This contribution was helpful to1 thankful Users |
5/9/2022 3:38 PM | |
Joined: 10/30/2018 Last visit: 12/18/2023 Posts: 9 Rating: (0) |
How did you solve it because i am facing same issues I write coil and there is no error. but my device is not responding on that as I need to on of the CB By same program I simulate mode save with plc and plc writing coil. but while connecting actual device it not working please help |
5/10/2022 9:35 AM | |
Joined: 8/3/2017 Last visit: 2/7/2024 Posts: 1085 Rating: (53) |
Hi dbvyas00, we need more information from you, at the moment it is quite hard to help you with so "many" information. Please tell us more about your setup and post, which Hardware you are using. Maybe a Screenshot will be useful to see, which steps you did try/ where you got stucked. Best regards |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
Follow us on