Industry Online Support
Technical Forum
5/10/2022 6:20 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS forum community, When migrating the function modules that are used in the S7-300, there are always questions. In this entry we have looked at the FM 350-1/FM350-2 module used in the S7-300. In order to declare a module in the S7-1500, the type and application of the encoders used must be considered. As a result, various possible solutions are available in the portfolio of the S7-1500:
An overview of the functions and further information to be observed during a migration can be found in the migration guide in Chap. 4.6 under technology features. All modules are available in the ET 200SP as well as in the ET 200MP design. The subject of counting, measuring and position detection for the S7-1500, ET 200MP and ET 200SP is described in more detail in the function manual. Another post here in the forum also deals with the SIMATIC S7-1500 technology modules. Note: The procedure described in this article refers to the time this article was created (as of July 2021). Best regards, SIMATIC International Technical Support Hub |
This contribution was helpful to1 thankful Users |
Follow us on