5/16/2022 8:08 PM | |
Joined: 3/12/2021 Last visit: 1/4/2024 Posts: 11 Rating: (0) |
Hello, I am looking for information regarding telegram 30. When configuring an S120 and utilizing telegram 30 in TIA Portal V16, the telegram occupies 12 bytes (6 Is & 6 Qs), but in list manual, pg 2252, it shows telegram 30 as 2 words (2 Is & 2 Qs). What and where is the extra data located in the 12 bytes? The SINAMICS S120 Function Manual Safety Integrated shows this as well and describes S_STW1 and S_ZSW1 using only 2 words (2 Is & 2 Qs). I am sure this is some inherent property of telegrams in which I do not know, but I have failed to find it in any manual. It seems the most I have been able to locate is the use of the premade functions in which the knowledge of the telegram structure is not needed. Thanks. |
Follow us on