5/1/2022 12:40 AM | |
Joined: 2/15/2022 Last visit: 1/21/2024 Posts: 3 Rating: (0) |
Hello, Anyone can help me? I have a canister with a weight load cell and an amplifier I need to tare the reservoir containing liquid or powder and tare it so I get the weight. Then when on valve open or a motor screw runs, I can measure the weight flow in gr/sec and adjust the screw feeding motor following a setpoint value? For example I have 2 Kg of powder in the canister and each second I have 7 to 8 gr of powder flow. I need to adjust to 10 gr/min so the motor increase or decrease rpm to get the correct flow. I have connected the logo with a load cell amplifier to get a 0-10Vvalue. Thank you if someone can put me on the rails. I know how to modify/ adapt but i am stuck with the logic. Attachmentpowder feeder.zip (508 Downloads) |
Last edited by: Yves CERDI at: 05/28/2022 12:16:11 |
|
Follow us on