5/27/2022 1:09 PM | |
Joined: 9/16/2021 Last visit: 2/8/2024 Posts: 30 Rating:
|
Hello Everyone, Currently working on :COMOS 10.4 with the 10.4.0.0 database We are working on P&ID and we want to change the way the label is displayed on the P&ID. There areoptions available in the "Graphical Options" on the right click(also in the attributes tab) on the function. I have observed strange thing that once I select "description" in the menu only description is shown and nothing else. Even the funtion name disappears. I am uploading screenshots to show the phenomena.I check the script in the standard table and there is nothing extra in the script to remove the label, just showing description using "DevAllDescription". These setting are coming from a standard table(@40|Y00|A10|B50|Y00N00336). Any help will be appericiated. Regards AttachmentFunction Symbol.zip (418 Downloads) |
Last edited by: Gin San at: 05/27/2022 13:10:21 |
|
Follow us on