6/9/2022 1:35 PM | |
Joined: 4/9/2008 Last visit: 3/25/2024 Posts: 5 Rating: (0) |
Hello! I get the same error message Failure (Bad values) when using a IOT2040. Some times it works and sometimes with this error message. I have just one S7 in node connected to one PLC and reading 38variables. S7 in node is set to: read all variables, emit only when value changes. I tried the flow on my PC, without any problems. I have a bit newer version of "S7 in" on my computer, had to install a a older version on the IOT2040. The rest of the flow is just some filter out the data that changed and then send data to mindsphere. I am also waiting on a IOT2050, But still, is it not possible to use IOT2040 to read 40 variables? Did you find a solution? /Anders ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/14/2022 14:06:29New subject after splitting |
|
Follow us on