6/19/2022 4:13 PM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (138)
|
Hello Amir Omidi, It is recommended to install the PCS7 Versions in released Operating systems. PCS7 V9.1 software is released with below mentioned OSs. Released operating systems: The following operating systems are supported in SIMATIC PCS 7 V9.1 SP1: • Windows 10 Enterprise LTSC 2019 - ES/Client • Windows Server 2019 Standard Edition - OS • Windows Server 2019 Datacenter Edition You can refer the link for more details (Section 3 Notes on installation): SIMATIC PCS 7 Process Control System PCS 7 Readme V9.1 incl. SP1 (Online) I hope it helps you! |
This contribution was helpful to1 thankful Users |
Follow us on