6/22/2022 4:50 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi, You can use the output "_MQ" [string] and connect it to a APL block like MonDiL and connect to: "BatchName". Then disable the block icon of the MonDiL and use an IO field to show the value. Or you can create a new block icon for MonDiL by yourself. The "BatchName" has s7_m_c attribute which means it's available on the OS. You won't need any custom block for this. |
Last edited by: Oreca at: 06/22/2022 16:51:35If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on