6/22/2022 5:05 PM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating:
|
Hi, Can you check the log (post it here). Its listed under \SIEMENS\WinCC\diagnose\APF_Engineering[xx].txt |
If I could help you, you can use the RATE button. Thank you. |
|
6/23/2022 7:11 AM | |
Joined: 6/23/2019 Last visit: 6/11/2024 Posts: 11 Rating:
|
Hello Oreca, Please find the log AttachmentAPF_Engineering_01.txt (166 Downloads) |
Automation isn’t a silver bullet, and it won’t fix your broken processes for you. |
|
6/23/2022 9:04 AM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating:
|
Hi, Hmm the logfile looks like it's not corresponding to your print screen. Did you check the settings in the APF engineering tool if they are correct? Is the function: "Permit activation on ES" disabled? (if so then OK) Are the blocks in the master library updated to the newest version? FB1775-1800, FB2080-2085, FC1775 Did you check the UDT's if they are still correct? The ranges were modified since V1.4 Maybe you can start the APF integrator first to check all archives first |
If I could help you, you can use the RATE button. Thank you. |
|
6/23/2022 8:03 PM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating:
|
Hi, I may have found a possible solution, but it depends if you use PCS7 V9.1 or higher. Which PCS7 version are you working at? The latest readme lists the following: "Restrictions in V2.1 SP1 • The new OS Project Property Option “Project directory is only shared for write-protected access“ coming along with PCS 7 V9.1 / WinCC V7.5 (enabled by default in new OS projects) is not yet supported by APF V2.1 SP1 and must be disabled for proper operation of APF Engineering Tool“. Let me know! |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
6/28/2022 9:28 AM | |
Joined: 3/14/2008 Last visit: 6/27/2024 Posts: 2075 Rating:
|
Hi, Did you change the FB numbers in the APF Engineering tool? If so, generating the SCL file will fail because the symbolic name does not match. In this case, you need to remove the name from the symbol list and generate the FBs again. But good that you solved this another way! Good luck |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on