6/30/2022 2:29 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi, For Drive And PLC Communication. Guide Video Reading Drive I/O and guide details for tech support TIA PORTAL SIMATIC PLC DRIVE COMMUNICATION CHECK OUT 2.1 General hardware setup Section Regards
Attachment109772227_SINAMICS_G120X_SpeedControl_TIAPortal_V1_0.pdf (443 Downloads) |
Last edited by: Jen_Moderator at: 07/01/2022 09:27:46Video embedded. PDF added as attachment. If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
6/30/2022 4:31 PM | |
Joined: 1/21/2020 Last visit: 1/25/2024 Posts: 5 Rating: (0) |
Hi Jack0004 and Stefan Arcularius, I did exactly that (Speed control via SinaSpeed) on a previous project and that works pretty good. However, using this method only gives me speed control of my drive and not much else. Because it only uses telegram 1, I don't have enough "space" for more data exchange. I also want to moniter motor current, motor voltage, etc. As Stefan Arcularius mentioned, the G120X does not have telegram 390. See attached. How do I connect the free transmit PDZ with parameter xxx? It would be nice if I could import those inputs into my project and use them as a PLC tag. Similar to the way you can with SIRIUS soft starters p730-p732 do not have CPU as an option for signal source. p738-p742 are not available on G120X. See attached. Attachmentpics.zip (427 Downloads) |
7/1/2022 9:18 AM | |
Joined: 1/21/2013 Last visit: 9/23/2024 Posts: 3122 Rating: (488) |
Hi Iwashere1st, I was hoping, some drive expert will post an answer. When you don't want to wait, try a Support Request. Kind regards |
7/2/2022 3:43 AM | |
Joined: 1/21/2020 Last visit: 1/25/2024 Posts: 5 Rating: (0) |
How to do tracing SINAMICS G120X parameters via SIMATIC PLC Sorry about that |
Last edited by: Jen_Moderator at: 07/27/2022 14:34:27Link optimized. |
|
Follow us on