6/30/2022 10:21 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello; The CP 1543-1 supports Modbus TCP, both as Client and Server. For confirmation, look at the last post in the following discussion amrcordg has prepard a screnshot that should clarify things (I have copied it in the screenshot below): https://support.industry.siemens.com/forum/ca/en/posts/modbus-tcp-with-cp1543-1-or-cm1542-1/138342 Hope this helps, Daniel Chartier |
This contribution was helpful to3 thankful Users |
8/16/2022 8:35 AM | |
Posts: 2 Rating: (0) |
HI , Can anyone share the sample Modbus TCP/IP program for (6GK7 543-1Ax00-0XE0 (CP 1543-1)) |
Follow us on