7/11/2022 1:02 PM | |
Joined: 8/12/2021 Last visit: 5/23/2024 Posts: 308 Rating: (29) |
Hi jortmbe! Occasionally, an error may trigger errors other than the communication status code. In these cases, it is interesting to save the first status value in an auxiliary flag to be able to identify the first error that originated in the communication. Have you tried to implement this logic? Does it return the same error? In the manuals of each version there are usually some Status error codes
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on