7/12/2022 12:55 PM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating:
|
Hi, For each signal you can have a quality bit which contains the status of the hardware signal. They are connected automatically by the driver wizard. |
If I could help you, you can use the RATE button. Thank you. |
|
7/13/2022 1:57 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi Vahid08, the detailed explanation of the address space for the ET 200SP HA DI 16x24VDC (6DL1 131-6BH00-0PH1) can be found in the manual SIMATIC ET 200SP HA digital input module DI 16x24VDC at the section Address space. With regards |
Follow us on