7/28/2022 2:57 PM | |
Joined: 3/31/2022 Last visit: 5/20/2024 Posts: 2 Rating: (0) |
Hello. I have the same problem. When trying to execute a command "Download to corrent project" in NetPro, the system returns an error: "The connection to the target module cannot be established". The S7online is set to the correct interface. [snip] ------------------------------------------------------------------------------------------ AttachmentScreenshots.zip (427 Downloads) |
Last edited by: Jen_Moderator at: 07/29/2022 09:59:29Links removed and files added as zip file. Last edited by: Jen_Moderator at: 08/01/2022 11:07:06New subject after splitting |
|
Follow us on