8/8/2022 8:46 AM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168)
|
Hello, Perhaps the following links might help: Transfer of S5 Time values (Timer data type) from an OP to the controller Sample program: S5 Timer in ProTool/Pro Operating the S5 timer via Operator Panel in the controller Best regards, Wizard |
This contribution was helpful to1 thankful Users |
8/8/2022 12:13 PM | |
Joined: 1/4/2019 Last visit: 6/1/2024 Posts: 60 Rating: (0) |
Thank you MR . Wizard the linear scaling is very helpful and i works very well Thanks a lot again |
Follow us on