7/31/2022 11:11 AM | |
Joined: 3/22/2022 Last visit: 11/1/2022 Posts: 69 Rating: (1) |
HI Sir How i can set axes compensation values? The Control is 840 D sl Rana Shafay |
7/31/2022 12:18 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello M. Shafay, There are different compensations & those are optional. User need to order those as per system application requirement. However I guess here you must be talking about lead screw pitch error Bi-direction compensation software, which is optional. Please check if it is installed on your system. Please refer attached which will help you to identify default & optional compensation softwares. Hope this helps. P. S. - If you need any additional or other information, please ask. |
Last edited by: PISCEAN 2010 at: 07/31/2022 12:32:51P. S. added |
|
This contribution was helpful to1 thankful Users |
7/31/2022 7:41 PM | |
Joined: 3/22/2022 Last visit: 11/1/2022 Posts: 69 Rating: (1) |
HI Sir
Yes I want to learn how to set Lead Screw measuring system error compensation Pitch error ., Back lash and Sag Compensation Multidirectional ( M54.M55o in pic). I have a little bit Experience of 840 D PL . But 840 Dsl is new for me. I want to know how i can modified the File and Find out the error. or how I can Set Accuracy of a Five or seven Axis Machine. Thanks in Advance Rana Shafay |
8/2/2022 10:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
HelloM. Shafay, Bi-directional compensation is optional which user need to purchase. Difference between bi-direction & uni-direction is - in bidirectional user can set & activate lead screw compensation in both direction whereas in uni-direction, user need to set average compensation values (not with respect to direction) User need to conduct axis accuracy by external laser measuring system & set compensation values based on error measured by laser measuring system. The compensation files are activated & error values are entered in table. Procedure is same as per 840D PL. Please refer SINUMERIK 840D sl expanded functions refer chapter 5.5.2 for lead screw error compensation. Hope this helps. |
Last edited by: Jen_Moderator at: 08/02/2022 13:12:18Link optimized. |
|
This contribution was helpful to1 thankful Users |
Follow us on