8/2/2022 3:29 PM | |
Joined: 6/8/2021 Last visit: 3/26/2024 Posts: 24 Rating: (0) |
Hi With my EMCO 345-2 with 810D control, I cannot carry out a zero offset of the C axis. I just doesn't work. I want to make parts that I need to machine on the other side after parting. Holes must be drilled (SPOS) and milled that are well aligned with respect to references in the first set-up. For the second setup, I use a feeler gauge to set a reference plane of the part parallel to the x-axis of the machine. For this I turn the main spindle by hand. The value of the spindle is then e.g. 55.12 degrees. With the help of the zero offset I just want to set the C axis in G54 to 0 now. So that the part is properly oriented to run the program. Attached are some pictures. When I type something in C it has no effect at all. At least not when using SPOS. Can somebody help me with it? Thanks
Attachmentresized.zip (279 Downloads) |
8/3/2022 10:03 AM | |
Joined: 1/19/2008 Last visit: 8/13/2024 Posts: 989 Rating: (63) |
Hi, You could try SPCON and SPCOF and then program moves as C. Pee |
8/3/2022 7:41 PM | |
Joined: 6/8/2021 Last visit: 3/26/2024 Posts: 24 Rating: (0) |
Thanks for the suggestions, I will look into it and try it on the machine in the next couple of days. |
Follow us on