7/24/2022 7:01 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello andrejx2013, Yes it is possible to use these i.e. 6SN1118-0NH11-0AA1 modules without CNC or PLC controller, simply by configuring digital inputs, pulse & drive enables & providing +/-10 V analog signals. Please note 6SN1118-0NH11-0AA1 is control card & not LT power module. The motors which you mentioned can be controlled by these 611U HR control card provided you have power LT module, 6SN112x-xxxx, compatible infeed module. Please refer SIMODRIVE 611 universal SIMODRIVE 611 universal E, Control Components for Closed–Loop Speed Control and Positioning & connection diagram chapter 2.3.1 for more information. Hope this helps. |
Last edited by: PISCEAN 2010 at: 07/24/2022 07:02:23Last edited by: Jen_Moderator at: 07/25/2022 11:00:39Link optimized. |
|
This contribution was helpful to
1 thankful Users |
8/10/2022 5:21 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Raise support request. or contact your nearest Siemens service/support center. |
Follow us on