4/23/2009 4:52 PM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838) |
Hello polle12, Please check the following links: How can you transfer a WinCC flexible project serially to a panel? How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Which USB master-master cables are recommended for the configuration download from WinCC flexible/ProTool to a Windows CE panel? And Also Please check that you have to use what we call the zero-modem serial cable for transfering your project to the panel. You can order one from Siemens MLFB: 6ES7901-1BF00-0XA0 SIMATIC S7,CONNECTING CABLE FOR HMI ADAPTER AND PC/TS ADAPTER, (RS232 / ZERO MODEM CABLE), 6 M 16.50EUR Also you can do it your self, just follow the following instruction and here's attached its pin assignment. Please note that you may only used shielded connector housings. The cable shield must be connected on both sides over a wide area with the connector housing and shielding line. AttachmentRS232 cable pin assignment.pdf (980 Downloads) |
Last edited by: Ayman Elotaify at: 4/23/2009 4:53 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on