8/27/2022 1:52 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Hi Hassan, I have few questions below: 1. Have you ever download successfully by using the same environment and setup? 2. Is this your first time setting up the project? 3. Have you configured the Host file with the IP address? 4. Is the workstation in workgroup or domain? Can you do a quick test: 1. exit all the download activities in ES and OS Server. 2. Perform a restart in ES and OS Server 3. After ES and OS Server restarted 4. At ES, Win+R (Run) -> key in "reset_wincc.vbs" 5. wait until "Ready" pop out dialog box appear 6. press ok and restart ES. 7. Repeat step 4 to step 6 in OS Server and restart. 8. perform your download again. Hope it is helpful to you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
5/30/2023 4:02 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by Gautham_Shetty is split to a separate thread with the subject Secondary server: Project stuck on Opening WInCC Project After OS Server Download. Best regards |
Follow us on