3/17/2017 12:28 PM | |
Posts: 146 Rating:
|
This is my example about communication CPU 1212C ver 4.0 with Indusoft web 8.0 ....this project just start and stop .. With tag in Indusoft web 8.0 (IWS8.0) u need add tag and the number of rack ..example in this project : tag: on_pump station : 192.168.1.100 : 0:1 ( where : the IP your CPU 1212C ; 0: rack 0; 1: slot :1) this is very important for u r tag active in IWS8. You need add the driver is : SIETH in Communication part of project exploer I can use web thin for mobile Ipad access..fot this simple example ... But i like use WEBUX in WinCC 7.4.... I love Siemens !
Note : remeber change from project2.zip to project2.rar and unrar this file ! AttachmentProject 2.zip (480 Downloads) |
Last edited by: xuanphu at: 3/17/2017 12:31:37 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on