9/12/2022 5:30 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating: (936)
|
Hi, So I guess you are trying to download the CFC program into the CPU? When you have setup a redundant Profinet network, where remote IO is connected to two Profinet networks, then you will need to have an additional license: S7 REDCONNECT. (6ES7653-2CX01-0XE0) See the following link: You will need to have setup two redundant CPU's up and running and this license will be installed on the SEC card of the CPU on both of them. You find more info on how to upgrade the SEC card with the redundant license in the following manual: Process automation with the CPU410 (page 65 on the V9.0 manual) |
Last edited by: Oreca at: 09/12/2022 05:47:54If I could help you, you can use the RATE button. Thank you. |
|
Follow us on