8/24/2022 8:05 PM | |
Joined: 10/6/2016 Last visit: 5/18/2024 Posts: 80 Rating: (1) |
Hi Dmitry Anyushin Do you possible tell me that wincc 7.5 sp1 with which version TIA PORTAL and which plcsime you can simulated? Thankful if guide me Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/25/2022 08:07:21New subject after splitting. |
|
8/25/2022 9:00 AM | |
Posts: 71 Rating: (28) |
Hello Ad_181......., WinCC 7.5 SP1 is compatible with S7-PLCSIM (V5.4SP8, V5.4 SP8 Upd1, V15.0, V15.1,V15.1 Upd1, V16.0) and TIA Portal (V16.0, V16.0 Upd1, V16.0 Upd2, V16.0 Upd 3, V16.0 Upd4, V16.0 Upd5, V17.0). You can check compatibilities using the compatibility tool: Compatibility information https://support.industry.siemens.com/kompatool/pages/main/index.jsf? Best regards, s7-mencey. PD: If this post helped you, don't forget to rate with 5 stars! |
Last edited by: s7-mencey at: 08/25/2022 09:02:14 |
|
This contribution was helpful to1 thankful Users |
Follow us on