9/20/2022 5:38 AM | |
Joined: 9/3/2008 Last visit: 8/9/2024 Posts: 927 Rating:
|
Hi abbasisahab Before you can import pictures/tags from your 5.0 project into your 7.4 project, you need to migrate the 5.0 project up to a 7.4 version. It has to be done in steps following this guide There is a note in the document stating: "You can only convert screens and libraries from one WinCC version to the next So the first step is to get it to 6.2 SP in order to upgrade to 7.2 and then up to 7.4. Best regards |
Michael |
|
9/20/2022 7:57 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating:
|
Hi! In order to complete the partner's answer, I provide the following information: You must migrate to different intermediate versions of WinCC, since a direct migration is not possible. The process is as follows: 1) V6.2 to V7.0: You would need this license upgrade: 6AV6381-2AB07-0AX3 2) 7.0 to 7.2: no licence would be required as the migration could be carried out during the trial period. A trial version of WinCC 7.2 is available to order under reference number: 6ZB5370-1DN70-2FA6. You should contact your Siemens supplier for the supply of this software (as it is not downloadable from Siemens). 3) 7.2 to 7.4 SP1: You will need this license upgrade: 6AV6381-2AB07-4AK3 Note: It is important that you install the various versions of WinCC on compatible operating systems when you carry out this migration process. You can check the compatibility of our software via our compatibility tool: |
If this post helped you in any way, please rate it positively. |
|
Follow us on