9/29/2022 10:46 AM | |
Joined: 12/20/2018 Last visit: 1/20/2024 Posts: 63 Rating: (0) |
Hi, I have attached the CPU Diagnose file below. I want this F1910 error from the driver to be masked by the plc. In other words, 1910 error should not cause BF and SF errors in plc. Should I use OB122 to mask the F1910 error from the driver? If so, what are the values I need to write in SFC36 here?AttachmentDiagnose_071130.txt (303 Downloads) |
Follow us on