9/27/2022 11:05 AM | |
Joined: 10/29/2014 Last visit: 11/29/2022 Posts: 25 Rating: (0) |
Hello I have the same problem. I have project in TIA V17. There is CPU 1512SPF, HMI TP700 and Simotion D445-2. I can connect online with PG, through ethernet. I can see online CPU, Simotion, but when I start the simulation HMI, I can see only ####. (Exactly in the HMI, there are all values.) I don´t understand what I should set in PC/PG interface else to solve this issue? Thank you for comments. Petr ------------------------------------------------------------------------------------------ |
Last edited by: Peetr at: 09/27/2022 11:07:54Last edited by: Jen_Moderator at: 09/28/2022 06:11:54New subject after splitting |
|
9/30/2022 12:27 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1732)
|
Hello Peetr perhaps the basic FAQ can help: https://support.industry.siemens.com/cs/de/en/view/109748099 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on