9/23/2022 7:30 PM | |
Joined: 2/12/2019 Last visit: 11/2/2023 Posts: 1 Rating: (0) |
Dear Members, I am working on Siemens Xworks for the configuration of Siemens BTU meters (Model NO. UH50). I have 89 Meters in total which are using M-Bus module for communication and are connected to Siemens Level Converter WTV531-GA5060 which act as Master for all these BTU meters. Now When i read this Level converter through Siemens ACT531 Readout software for these BTU meters, I got all the Data from these Meters. For Integration of these BTU meter to Desigo CC. I am using PXC001E.D Controller and I have attached an Rs232 Cable from this Siemens Level Converter (ABC) point and connect it to PXC001E.D controller Serial Port. I have configured Data Points in point configurator for all these Data Points but when tried to read these Data Points Online, It shows Zero Values. Kindly guide me how to get accurate Values of these BTU meters in X works. I have Attached a word File in which i have shown the configuration and the results which i got, I have a deadline to complete this integration next week. Zeeshan Ahmed Email:[snip] AttachmentXworks Working and Probelm occur.docx (401 Downloads) |
Last edited by: Jen_Moderator at: 09/26/2022 07:05:47E-Mail address removed. |
|
Follow us on