10/12/2022 5:27 AM | |
Joined: 5/6/2010 Last visit: 9/21/2024 Posts: 1978 Rating: (276)
|
Hello, if I understand it right, you need for your network at every floor
Then you should think about a switch at every floor, e.g SCALANCE XB205-3 (6GK5205-3BB00-2AB2). Then can you build with the fiber optic a ring structure in your buildings and at the RJ45-ports can you connect the ET200SP and the HMI-panel. This solution is not the cheapest, but when you use managed switches it's easier to maintnenace the complete system and also for a easier troubleshooting. For the configuration is the "best case" to use the TIA Slection Tool. regards |
This contribution was helpful to1 thankful Users |
Follow us on