10/11/2022 10:36 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello, even for connection to the Profibus network, the MPI cable supplied with the CP is often sufficient, but it is more convenient, especially at higher speeds, to use a Profibus cable. This is the RS485 type by default. On the CP side, you need a 9-pin D-Sub connector. On the opposite side, you need a connector according to the type of interface on the device to which you will connect - by default it is the same one, but it can be different, for example M12 type. You can order a pre-assembled cable, e.g. this, or assemble your own from individual components as needed. Sydney |
This contribution was helpful to1 thankful Users |
Follow us on