10/13/2022 12:11 AM | |
Joined: 2/25/2022 Last visit: 10/13/2022 Posts: 9 Rating: (0) |
Hi: Any word on this? G |
10/13/2022 5:47 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, I don't know the reason for this to be honest. I made several tests with 32GB cards and different tools to write the Example Image to the card - no success. If I recall correctly, R&D told me that it works using dd to flash the image to the card. I also can't explain why it works when touching the file manually. You could open an issue on github with this description, maybe the developer can make use of this information to understand the issue and try to find a solution in the future. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on