10/18/2022 12:22 PM | |
Joined: 3/11/2019 Last visit: 5/17/2024 Posts: 1417 Rating: (255) |
Hi, if no message to missing software packages are shown, this should not be an issue for the crash. But as i can see on the screenshot, a very old version is used (STEP 7 V5.6 + hotfix 1). In the meantime STEP 7 V5.6/Professional 2017 with servicepack 2 + hotfix 9 is available. At first i would recommend an update to the current version (no other license needed). regards sancruz STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial DownloadDownload Hotfix 9 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2 |
Feedback appreciated, please rate |
|
Follow us on