11/1/2022 10:24 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Dear All, I am using VLT Microdrive Danfoss. I need technical support for running this VFD from PLC S7 1200. 1) Terminals for Analog frequency command? 2) Parameters to enable switching between Jog/Remote Mode 3) above 2 points are enough ? Or I have to give Digital start command along with analog reference too? Pls help me with complete procedure to RUN this VFD from PLC.. Thanks Gajendra D S ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/02/2022 04:56:14New subject after splitting "Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
11/2/2022 4:57 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Danfoss Drive control from S7 1200 is published within the conference SIMATIC S7-1200. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on