11/4/2022 12:50 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello umutorkan a float datatype in SQL should be a Real datatype in HMI -> LINK Try a real Tag. And you can ry to check if the sql statement gives back a propervalue with the systemfunction ShowSystemAlarm in the script. Then you see in the alarm view if the value comes back as you need. bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on