11/4/2022 3:29 PM | |
Joined: 4/21/2022 Last visit: 4/14/2024 Posts: 96 Rating: (0) |
HI A question mark appears next to the blocks. what is the reason In the photo below, I specified the issue best regard |
11/4/2022 5:40 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, You have interconnected the EN input. EN is the enable of the block so if EN=0, the block logic is not executed. But because you have interconnected the EN, the system can't determine if the block is executed and therefore shows a question mark. If you set EN to 0 permanently, then a red exclamation Mark is shown indicating the block is nog executed. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on