11/2/2022 10:27 AM | |
Joined: 2/17/2020 Last visit: 9/24/2024 Posts: 1067 Rating: (192) |
Hi ZerkratztTV, Yes, but you need to establish a VPN tunnel. |
A rating will be well appreciated. |
|
11/3/2022 2:47 PM | |
Joined: 2/17/2020 Last visit: 9/24/2024 Posts: 1067 Rating: (192) |
Sure. The VPN connection can be realized with various components. To make the SIMATIC HMI Panel accessible via the VPN connection, the used router must be entered as standard gateway in the property "PROFINET interface [X1] > Ethernet addresses” of the panel in the TIA project. Look at this documentation too: Overview: Secure Remote Access with VPN |
A rating will be well appreciated. |
|
11/10/2022 9:36 AM | |
Joined: 8/3/2009 Last visit: 9/25/2024 Posts: 13788 Rating: (1741) |
Hello ZerkratztTV Here you will also find a lot of information about accessing Sm@rtServer from different Subnet or even WAN https://support.industry.siemens.com/cs/de/en/view/109476153 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on