11/11/2022 9:53 AM | |
Joined: 8/22/2022 Last visit: 7/18/2024 Posts: 10 Rating: (0) |
Hi, The programme that I have written now repeats how I would like - I was wondering if anyone can help me with one last thing. I would like to use two inputs - stop button and reset into the programme. Stop - stops the cycle as it is. Reset - only reset once sequence has stopped and then energizes Q1 - Q2 - Q3. then once started the sequence carries on from Q4. I'm open to any improvements my programme needs. thank you in advance Attachmentsequence for laster cutter strpping bench.zip (630 Downloads) |
Follow us on