11/9/2022 4:48 PM | |
Joined: 2/17/2020 Last visit: 9/19/2024 Posts: 1061 Rating: (192) |
Hi again, There doesn't seem to be a specific Communication Service Package (CSP) for connection to Schneider PLCs, so it may not be released or system-tested. However, I recommend you follow the steps below and use the "Modicon Modbus TCP/IP" driver in the connection: Communication Service Packages (CSP) for WinCC im TIA Portal |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
11/14/2022 7:24 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13745 Rating: (1731)
|
Hello wxflint If your Schneider PLC supports a OPC UA Server then you also could use OPC UA for communication. There are also usecases for this like in this example (unfortunately no Schneider PLC): LINK Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on