11/12/2022 12:24 PM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4444 Rating: (928) |
Officially there are two references: It is worth mentioning that the OP7 was replaced by the OP77. So what you are looking for in the references is for the OP77 replacement. Do not blindly follow the official suggestions however flawed. The KP400 Basic has the form factor but does not have a DP port. The KP400 Comfort is then the next option. The SMART product range (available in India) is not mentioned. The best cost effective + modern replacement would be the KTP700DP Basic (6AV2 123-2GA03-0AX0). None of the options are drop in replacements, so this options is viable. Engineering will need to be done from scratch. It might be worth your while to check 3rd party (non-siemens) offerings. ~ |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
11/14/2022 7:31 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello here is also a Migration guide for the first step from Protool to WInCC flexible: https://support.industry.siemens.com/cs/ww/en/view/18796902 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on