11/14/2022 1:32 PM | |
Joined: 11/14/2022 Last visit: 5/10/2023 Posts: 1 Rating: (0) |
Does anybody know about the implications of changing IP addresses?. I have a PCS7 system with two controllers (one for safety) and two operation stations (one of them works as engineerign station also). Is there additional job required besides the IP address change?. Is it as simple as changing the addresses? Is it going to be required to download hardware or something else after addresses are changed? I would appreciate your comments regarding this issue... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2022 06:38:03New subject after splitting |
|
11/15/2022 7:23 AM | |
Joined: 1/11/2019 Last visit: 10/7/2024 Posts: 764 Rating: (150)
|
Hello Sam,
Hence, I may not recommend to disturb the system if you do not know the complete steps. Changing the IP address may cause OS disconnection if you miss the configure, compile and download steps to all configured station. To get some more information about how to setup a PCS 7 project in general (AS, OS, clients) you should have a look in the PCS 7 compendium. This is a very good guideline will answer a lot questions. You can find in the below link: |
Follow us on