11/15/2022 3:16 PM | |
Joined: 7/19/2022 Last visit: 9/25/2024 Posts: 384 Rating: (62) |
Hi prozmanic, The problem is that the backup you bring from the screen is not editable. So if you have brought the PLC program and you have modified something (for example variable names (PV), IPs ....) it is very likely that this has caused the loss of connection between PLC and Panel (####). You would need to have the original project to make changes and be able to upload them to the screen.
|
Last edited by: JBS98 at: 11/15/2022 15:19:51If this Information really helps, you could use the Rate function |
|
Follow us on