11/22/2022 9:39 PM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating: (13) |
Did you set the "terminal bus" to the first position in Simatic Shell? Is the redundancy configured correctly in Simatic Shell? Hi Mr Oreca, in the engineering station / Simatic Shell / Redundancy Settings / the network card that will do the redundancy with both servers should appear or this should only appear in the Simatic Shell of each server (main and secondary?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/23/2022 07:40:10New subject after splitting |
|
11/23/2022 7:40 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Redundant Server can´t open the Runtime is published within the conference Process Control Systems SIMATIC PCS 7. Best regards, |
Follow us on