11/24/2022 2:19 PM | |
Joined: 10/2/2020 Last visit: 4/5/2024 Posts: 3 Rating: (0) |
Hello, Did you find a solution to your problem? Because I have the same problem I can't load the HMI program with TIA Portal going through Smartserver application. TIA Portal does not find the HMI Panel which I can ping with windows command. I start to believe that downloading a HMI program remotely does not work. I can load the PLC program remotely though. If someone can confirm. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2022 07:24:36New subject after splitting |
|
11/25/2022 9:32 AM | |
Joined: 5/30/2022 Last visit: 4/22/2024 Posts: 520 Rating: (85) |
Hi Lolo1803: Are you getting an error message? If yes, please attach a screenshot. Please check this Application Example to be sure that you configue well Sm@rt Server: Remote Access to SIMATIC HMI Operator Panels |
Last edited by: Hazard_7 at: 11/25/2022 09:34:54If this information really helps, you could use the Rate function. |
|
Follow us on